TivaWare™ for C Series is an extensive suite of software designed to simplify and speed up embedded application development using Tiva C Series MCUs. The suite includes the peripheral driver library, graphics library, USB library, and the sensor library, which includes several APIs to configure and initialize different peripherals of the Tiva C Series MCUs. These libraries come with the source code which is written mostly in C, and are pre-compiled for use 'as-is' and can also be adapted as desired. TivaWare for C Series also includes a boot loader, several code examples, and third party packages that allow the designer to focus on their application development and not so much on 'how to set up the MCU.'