Typical applications include most electronic, hand-held devices that require a means to store and retrieve data. It should be noted that the DM3C series connector is mainly used at an OEM level as it is installed by the OEM and end users typically do not have access to the connector or microSD card. Applications may include hand-held games where there is no need for a user removable card or in some in-car navigation systems that need microSD storage that is factory installed. However, the use of DM3C is not limited to these types of applications.