To speed up development time, ams OSRAM offers demoboards and software for the AS1115. There are various types of boards available depending on the end application requirements. The AS1115 demoboard for user interfaces shows the mixture between single LEDs, 7 segment LEDs, and key read back with simple to use software. This software also shows the required I²C data transition in a separate window to allow transparent programming. For the AS1115 demoboards, either an existing I²C master can be used or, if ams OSRAM demoboard software is used, a separate USB Box must be ordered.