Maker.io main logo

Qwiic Magnetometer (MLX90393) Hookup Guide

139

2018-05-22 | By SparkFun Electronics

License: See Original Project Arduino Qwiic Raspberry Pi SBC

Courtesy of SparkFun

Introduction

The MLX90393 is a tri-axial magnetic sensor capable of sensing very small fields (like the Earth’s magnetic field) while behaving as one would want and expect during saturation in larger fields (like a nearby magnet). It turns out the favorite HMC5883L and other such sensors that are intended for compass applications have a low dynamic range but also strange and undefined behavior in large fields. Ted Yapo did an incredibly extensive characterization of the sensor over on Hackaday. He published his controlled experiments testing a few sensors and found the MLX90393 to be superior.

The MLX90393 can be used as a compass sensor but also works well as a non-contact controller (joystick), flow meter (with magnetic impeller), or a linear actuator position sensor. The breakout board is also a part of SparkFun’s Qwiic system, so you won’t have to do any soldering to figure out what the magnetic fields look like.

SparkFun Triple Axis Magnetometer Breakout

SparkFun Triple Axis Magnetometer Breakout - MLX90393 (Qwiic)

 

In this hookup guide, we’ll get going by getting some basic readings from the sensor, then look at how to configure the sensor on different I2C addresses.

Required Materials

To get started, you’ll need a microcontroller to control everything in your project.

Now, to get your microcontroller into the Qwiic ecosystem, the key will be one of the following Qwiic shields to match your preference of microcontroller:

You will also need a Qwiic cable to connect the shield to your magnetometer, choose a length that suits your needs.

Or, here’s the wishlist to follow along exactly with this guide:

Suggested Reading

If you aren’t familiar with our new Qwiic system, we recommend checking out our overview:

WHAT IS QWIIC?

We would also recommend taking a look at the hookup guide for the Qwiic Shield if you haven’t already. Brushing up on your skills in I2C is also recommended, as all Qwiic sensors are I2C.

  • I2C: An introduction to I2C, one of the main embedded communications protocols in use today.

  • Serial Terminal Basics: This tutorial will show you how to communicate with your serial devices using a variety of terminal emulator applications.

  • Qwiic Shield for Arduino & Photon Hookup Guide: Get started with our Qwiic ecosystem with the Qwiic shield for Arduino or Photon.

Hardware Overview

Let’s look over a few characteristics of the MLX90393 so we know a bit more about how it behaves.

Let’s look over a few characteristics of the MLX90393

Pins

The characteristics of the available pins on the magnetometer are outlined in the table below.

Pins

Optional Features

The Qwiic MLX90393 has onboard I2C pull up resistors, which can be removed by removing the solder from the jumper highlighted below. Only remove this solder if you are using your own pullups on the I2C lines.

Qwiic MLX90393 has onboard I2C pull up resistors

The I2C of the Qwiic Magnetometer can be changed using the A0 and A1 jumpers on the back of the board. Simply cut the traces connecting each pad to ground (0) and solder the other side to connect it to 3.3V (1).

I2C of the Qwiic Magnetometer can be changed

To operate the Qwiic Magnetometer in SPI mode, cut the chip select trace jumper (labeled below) and ensure that the CS pin is then connected to ground.

operate the Qwiic Magnetometer in SPI mode

Hardware Assembly

If you haven’t yet assembled your Qwiic Shield, now would be the time to head on over to that tutorial.

QWIIC SHIELD FOR ARDUINO PHOTON HOOKUP GUIDE

With the shield assembled, SparkFun’s new Qwiic environment means that connecting the sensor could not be easier. Just plug one end of the Qwiic cable into the Magnetometer breakout, the other into the Qwiic Shield of your choice and you’ll be ready to upload a sketch and figure out what the magnetic fields look like. It seems like it’s too easy to use, but that’s why we made it that way!

Connected Magnetometer

Example Code

Before we get into programming our Magnetometer, we’ll need to download and install the magnetometer library. Ted Yapo has written a library to control the Qwiic Magnetometer. You can obtain the .zip for this library using the below button. Never installed a library before? That’s ok! Check out our tutorial on installing Arduino Libraries.

DOWNLOAD THE MLX90393 LIBRARY

Note: This example assumes you are using the latest version of the Arduino IDE on your desktop. If this is your first time using Arduino, please review our tutorial on installing the Arduino IDE. If you have not previously installed an Arduino library, please check out our installation guide.

Since this isn’t a SparkFun library, the example sketches are not included, so you’ll have to download those from the Github page by clicking the below button. The example sketches are located in software

DOWNLOAD THE MLX90393 GITHUB REPO

Go ahead and unzip these examples to a location of your choosing and open Example 1 - Basic Readings.

Example 1 - Basic Readings

Once we have our first example opened up, let’s look at how things are structured as we set up our sensor. First, we create our sensor, and then an array of floats to contain our data.

Copy Code
MLX90393 mlx;
MLX90393::txyz data; //Create a structure, called data, of four floats (t, x, y, and z)

Then in our setup loop, we must initialize our sensor, notice the delay afterwards, this gives the sensor time to initialize before we start attempting to talk to it.

Copy Code
mlx.begin(); //Assumes I2C jumpers are GND. No DRDY pin used.
delay(1000); //Allow the sensor to initialize.

Once the sensor is initialized, our void loop() will read the data from our sensor into data, the array of floats we created earlier, and print it over serial to our serial monitor. Opening up your serial monitor to a baud rate of 9600 should display output similar to that shown below. The numbers are in units of µT. For scale, the magnetic field of the Earth ranges from 25 - 65 µT.

the magnetic field of the Earth ranges from 25 - 65 µT

Example 2 - Configure Sensor

Go ahead and open Example 2 from the location you saved it in. The only differences between this example and the previous one are in the setup() function. Notice how we now call the begin() function with 3 arguments, which are the value of the A0 jumper, the value of the A1 jumper, and the pin that we’ve connected to INT. The below code assumes that the A0 jumper has been cut from ground and soldered to 3.3V and that A3 is connected to the INT pin (sometimes referred to in the datasheet as the DRDY or data ready pin).

Copy Code
byte status = mlx.begin(1, 0, A3);

If we must change the address of our magnetometer due to overlapping addresses, ensure that the values we pass into begin() match up with the values of our address jumpers. The MLX90393 also has a ton of different ways to change the sensor behavior. You can set the gain, resolution of the x, y and z channels, oversampling rates, and even offsets of your x, y, and z channels. In this example, however, we set the gain to 1 and the resolution of our x, y, and z channels to their finest setting, 0.

Copy Code
mlx.setGainSel(1);
mlx.setResolution(0, 0, 0);

A table showing the different possible resolutions of the sensor for the X and Y axes is shown below. These can be selected using the setGainSel(uint8_t gain) and setResolution(uint8_t x, uint8_t y, uint8_t z) functions. All resolutions are in units of µT/LSB.

XY Axis:

XY Axis

Shown below is the table containing the possible combinations for resolutions on the Z axis. Once again, units are in µT/LSB

Z Axis:

Z Axis

Since we are simply connecting our magnetometer on a different address, our output should be similar to the one in the first example.

Resources and Going Further

For more information, check out the resources below:

Mfr Part # 14571
QWIIC MAGNETOMETER MLX90393
SparkFun Electronics
17,18 €
View More Details
Mfr Part # 13975
REDBOARD ATMEGA328 EVAL BRD
SparkFun Electronics
19,36 €
View More Details
Mfr Part # 13907
SPARKFUN ESP32 THING
SparkFun Electronics
26,55 €
View More Details
Mfr Part # SC0022
SBC 1.2GHZ 4 CORE 1GB RAM
Raspberry Pi
30,12 €
View More Details
Mfr Part # 14352
QWIIC SHIELD FOR ARDUINO
SparkFun Electronics
6,67 €
View More Details
Mfr Part # 14459
QWIIC HAT FOR RASPBERRY PI
SparkFun Electronics
5,98 €
View More Details
Mfr Part # 14477
QWIIC SHIELD FOR PHOTON
SparkFun Electronics
5,59 €
View More Details
Mfr Part # 14428
QWIIC CABLE - 200MM
SparkFun Electronics
1,34 €
View More Details
Mfr Part # 14429
QWIIC CABLE - 500MM
SparkFun Electronics
1,88 €
View More Details
Mfr Part # 14427
QWIIC CABLE - 100MM
SparkFun Electronics
More Info
View More Details
Mfr Part # 14426
QWIIC CABLE - 50MM
SparkFun Electronics
More Info
View More Details
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.